Part Number: SN65DPHY440SS
Hi,
For the RST pin, it is mentioned that it is critical to reset the PHY after VCC. In our prototype, we have pulled the RSTN high using VCC, and currently, it is working fine. Is there a specific need to modify it according…
Part Number: SN65DPHY440SS Hi Ti engineer,
Our company encountered the following problems when using sn65dphy440ss verification: 1, signal source-turn-board -MIPI display screen, the picture is normal; 2, add a turnboard with sn65dphy440ss chip,MIPI display…
Part Number: SN65DPHY440SS Hello,
In our a project , we used SN65DPHY440SS and needed to do an eye dagram simulation for D-PHY signal.
We downloaded the RX and TX snp file.
Our application is as follows:(the parts circled in red need to be simulated)
…
Part Number: SN65DPHY440SS I am evaluating the compatibility between SN65DPHY440SS and our existing MIPI board. I hope to control the enabling of each channel's LP and HS modes through I2C. The register mapping in the datasheet does not seem to be complete…
Part Number: SN65DPHY440SS Hello team
I like to use a 500mm cable between the processor and the display. Using a high quality TwinAx cable from 3M the insertion loss is <5dB at the desired frequency and can be compensated by the SN65DPHY440SS. However…
Part Number: SN65DPHY440SS Hello,
One customer used SN65DPHY440SSRHRT for his application, LP/HS is normal without connected load.
But when connected load, LP is normal, while HS has no output.
Please help to analyze.
Best regards
Kailyn
Part Number: SN65DPHY440SS Hi TI Team,
We are using SN65DPHY440SS re-timer part for an internal design and we face an issue with respect to routing aspects from re-timer IC to the sink connector. Swapping of data lanes at the re-timer IC end would resolve…
Part Number: SN65DPHY440SS Hello team,
On the datasheet, this device has receive equailzer, which can be enabled up to 4dB at 500MHz.
This means that if the input signal was attenuated by 4.5dB along the data line, this device can output a signal with…
Part Number: SN65DPHY440SS Person in Charge,
We are planning to use your evaluation board of this device for our study.
Could you let me know the product number of camera which we can use on this evaluation board.
Best Regards,
Akira