Part Number: SN65DSI83Q1-EVM
Dear Team,
May I know you have any reference code for
SN65DSI83Q1-EVM
I mean some source code or example code etc
Regards
HARI
Part Number: SN65DSI83Q1-EVM Hi,
I'm trying to use the SN65DSI83Q1-EVM board to assist in doing some display electronics and I need to make an adapter board that connects to both J4 and J6 (both are Samtec connectors) so that I can interface with my other…
Part Number: SN65DSI83Q1-EVM Hi TI team,
We have a LCD flickering issue on automotive head unit application. Some of the DSI83 IC has very high chance to reproduce LCD flickering, like 4/5.
I am now go through the slla356 trouble shooting guide. Can you…
Hello Zach,
i was looking for the schematic and the board file of the SN65DSI83Q1-EVM, i have the blue version of the PCB. The schematic in the document on the TI-Page with the name: " SN65DSI83, SN65DSI84, and SN65DSI85 EVM User’s Manual and Implementation…
Part Number: SN65DSI83Q1-EVM Good day
I am currently trying to connect a 3.3V LVDS TFT LCD Panel to the SN65DS183Q1-EVM board. The SN65DS183Q1-EVM is 1.8V LVDS level and the development board does not provide a level translator. Is this even possible? the…
Part Number: SN65DSI83Q1-EVM Other Parts Discussed in Thread: SN65DSI83 Hello.
Test condition.
LCD : 800*480
using mipi 2lane, 24BPP
LVDS clock is defined by panel as 30MHz.
DSI clock is 180MHz.
CPU : MSM8974
MSM8974 MIPI <-> SN65DSI83Q1-EVM
DSI…
Part Number: SN65DSI83Q1-EVM Can you please provide information on this Samtec HDR-128291-XX breakout board referenced in the document and where I can purchase it?