Part Number: SN65DSI86 Hello.
We are struggeling to get the DSI interface working. When connecting the bridge to a monitor @ 640x480/60Hz, we get a picture that turns on and off.
The DSI uses only channel A, four lanes of data.
We have checked the DSI…
Part Number: SN65DSI86 Hello:
The SN65dsi86 adapter chip has a timing requirement, which requires flashing a black frame before the LCD screen lights up and a black frame before the sleep screen goes out,
Namely, adding a black frame during sleep and…
Part Number: SN65DSI86 Hi,
I am developing with STM32 L4 or U5 MCU.
Could someone share how you got (LTDC, DSI, DMA2D, and SN65DSI86 Configuration) this bridge working with STM DSI?
Any help will be much appreciated.
Thanks
Part Number: SN65DSI86 Hi.
I have a question regarding termination of the MIPI-DSI lines for the SN65DSI86 MIPI-DSI - eDisplayPort bridge.
The question is regarding the MIPI-DSI input lines.
Does the differential MIPI-DSI input lines have an internal…
Part Number: SN65DSI86 mopo to DP bridge device and that need support to 4K, 60Hz HBR3 , do you have recommend device can promote to customer ? thanks.
Part Number: SN65DSI86-Q1 Hi TI teams,
The eDP lane assignment and lane polarity can be configured at the same time through 0x59 and 0x5A register. The connection is showed as below. Is it correct ?
Part Number: SN65DSI86-Q1 Other Parts Discussed in Thread: SN65DSI86 , TEST2 The following error occurs when imx8mm is used for SN65DSI86, Linux5.10
ti_sn65dsi86 3-002d: [drm:ti_sn_bridge_enable] *ERROR* Link training failed, link is off (-5)
This is my…
Part Number: SN65DSI86 We are able to communicate to the bridge using i2cset and invoke built in colorbar is display on LCD panel, however we are not able to get the mipi_dsi output on the LCD This are the below log which we are getting on drm and we don…
Part Number: SN65DSI86-Q1 I 'm going to select the part for MIPI to eDP
The LCD to be used has the following specifications.
-. 3840x2160 resoluton, eDP 1.4 interface, 10bit Color Depth, min 350nit @SDR, HDR1000
so. I want an IC that supports the features…