Part Number: SN65HVD10-EP Other Parts Discussed in Thread: DP83867E , TPS6594-Q1 Hello,
I am looking for a thermal model of the following device:
- RS485, part number: SN65HVD10-EP
The model need to be in a .tzr-format to be able to import them in the simulation…
Part Number: DP83867E Other Parts Discussed in Thread: SN65HVD10-EP Hello,
I am looking for thermal models of the following three devices:
- Ethernet, part number: DP83867ERGZ
- PMIC, part number: TPS6594
- RS485, part number: SN65HVD10-EP
The models need…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: SN65HVD10-EP , SN65HVD10 Hello,
I am looking for a thermal model of the following device:
- PMIC, part number: TPS6594-Q1
The model need to be in a .tzr-format to be able to import them in the simulation…
Part Number: SN65HVD10-EP Other Parts Discussed in Thread: SN65HVD10 , THVD2450 , THVD1450 I am analyzing a SN65HVD10MDREP in a circuit that has external protection on the outputs of the device. I need the characteristics of the internal 16V clamps to determine…
Part Number: SN65HVD10-EP Other Parts Discussed in Thread: SN65HVD10 Is the IBIS model for the non-EP version of the SN65HVD10 valid for use with the -EP version? Devices are in the same package.
Part Number: SN65HVD10-EP What happens if A and B are tied to ground?
Esp in the cases where
1) D has a value and DE is high (enabled)
2) /RE is low (enabled)
Unfortunately, we do not have a 3.3 quad line driver with enough absolute max headroom for TVS diode for lightning suppression.
I did search through our other EP interface offerings. We do not have any 3.3V quad RS485 transceivers. We do have one…