Part Number: SN65HVS880 Other Parts Discussed in Thread: SN74HCS164
Hi team,
My customer is considering SN65HVS880 for digital input application in motion controller, do you have any digital output device to recommend, just similar with SN65HVS880? Thanks…
Part Number: SN65HVS880 Hi TI Team,
I would like to check if the following parts below are able to go through washing process (DI water).
Please provide any relevant supporting document if possible.
SN65HVS880PWPR
SN74LV4052ADR
ADS8688IDBTR
TXS0102D…
Part Number: SN65HVS880 For any of the inputs, if it is a floating node (for example when a switch is on, the input will receive 24V. If the switch is off, then it will be an open circuit) will the serializer interpret it as a logic low signal? Specifically…
Part Number: SN65HVS880 How to calculate device power dissipation for different values of Rlim ?. Worst case power dissipation in data sheet is 2591mW is quite higher. Is there any ways to reduce this by increase Rlim and load currents
In my circuit,…
Part Number: SN65HVS880 I need directly connect SN65HVS88x to 3.3V powered microcontroller with 5V tolerant inputs. Will the CE,CLK, LD, SIP inputs of the SN65HVS88x accept 3.3V logic signals? I cannot find logic input treshold levels for these pins in…
Other Parts Discussed in Thread: SN65HVS880 Hello
Sorry I dont know if this is the right forum ;
we use SN65HVS880 at 24volt ;
we leave REx pin floated ; is that ok ? or we should connect them to ground if we dont need leds?
we used RLim : 25k ohms and…
Hi Juan,
I unfortunately do not have a good solution to recommend for NPN inputs at this time. The HVS880 device would be able to properly sense high/low levels if an external pull-up resistance were used, but would not be able to limit the current…