Part Number: SN65HVS881 Hi Folks,
According to the datasheet: https://www.ti.com/lit/ds/symlink/sn65hvs881.pdf?HQS=dis-mous-null-mousermode-dsf-pf-null-wwe&ts=1679662106302&ref_url=https%253A%252F%252Fhu.mouser.com%252F
Please consider the Figure…
Part Number: SN65HVS881 Other Parts Discussed in Thread: TIC12400-Q1 I have a customer currently using the MC33978. Our SN65HVS881 is not pin2pin with it and hard to push them to evaluate. Do we have any selling points or a comparison table with SN65HVS881…
Part Number: SN65HVS881 Hi team,
My customer use many pcs SN65HVS881 in their I/O board.
it have production. But they found SN65HVS881 5VOP pin short circuit to GND, which often happen. Below is their SCH.
Do you have any suggestions?
Thanks!
Part Number: SN65HVS881
E2E,
We have a question for you: the debounce filter can be setup with DB0/DB1 pins. Can they program the debounce filter during normal operation/on the fly ? or they should do it only at start up?
Do we have any device similar…
Part Number: SN65HVS881 Hi, staff Please ask questions on SN65HVS881PWPR (Serializer).
When IP terminal is not used (not used), Is there any problem with the RE terminal open?
best regards cafain
Part Number: SN65HVS881 Hi,
I am currently using 2 sn65hvs881 chip, in daisy chain, for getting 16 bit input for development purpose. I am using raspberry pi for the controller part. currently, i have connected the chip to rpi using a mosfet (bss138…
Part Number: SN65HVS881 Hi,
According the datasheet, in a type-2 switch application with two inputs in parallel one of the REx pins should be connected to the LED and the other one to GND, why can't it be left unconnected?
Regards,
Part Number: SN65HVS881 Hi All,
We have selected this SN65HVS881 IC for our applications.
But, we want to know, whether this IC will support for multiple bit parity error check ?
If this IC is not supported, how to handle the multiple bit parity error…
Part Number: SN65HVS881 Other Parts Discussed in Thread: ISO1212
In the reference design, the RE pin is directly connected to the LED.
But it is well known that what color LEDs can be driven is related to the drive voltage and current.
How do I determine…