Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDS2 , SN65ELT20 , SN65ELT21 , SN65ELT22 , SN65LVELT23 Hello, I am trying to use AFBR-5805ATZ in custom application where no high speed communication is needed. I just want to send pulses to the transmitter…
Hello Rayna,
I apologize for the delay on this.
With the device being released +20 years ago, our design/verification parameter differs from what it is today. Back then some min and max timing specs were not considered.
Unfortunately, we don't have the…
Part Number: SN65LVDS1 Dear TI,
what is psi j-c (characterization parameter junction-case) or psi j-t (junction - top) in °C/W for package SOT 23-5?
Thank you.
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65LVDS2 , Hi team,
I'm looking for SN65LVDS2/4 companion LVDS driver which can work with 2.5V.
The application is SPI-to-LVDS bridge for the board-to-board communication.
For the sake of limi…
Part Number: SN65LVDS1 Hello there,
I use the SN65LVDS1 as the clock buffer to replace FIN1001M5X.
as i tested, the differential output signal has a 60mV overshot like shown in the image below. i have attached the schematic, please help me to understand…
Part Number: SN65LVDS1 Hello, My customer would like to simulate SN65LVDS1 SOIC(8) package using ibis model. However, it seems that the ibis model at TI.com is for only for SOT(5). TI does not support SN65LVDS1 SOIC(8) ibis model? Best regards, K.…
Part Number: SN65LVDS1 Hi Team,
Can you please check and advise with following request:
"
I need SN65LVDS1DBV junction-to-board thermal resistance value. There is not enough information available in the datasheet. If you can find this information…
Part Number: SN65LVDS1 Hi team, Good day.
Does the SN65LVDS1 provide an output similar to the input supply? For example, if we have a 2.5V input and supply the device with Vcc= 3.3V, is the differential output effectively 3.3V LVDS, or is the output 2.5V…