Part Number: SN65LVDS822 Other Parts Discussed in Thread: SN65LVDS86A Hi,
Greetings.
Looking for the following part in "SN65LVDS822" in Automotive or Military grade (having operating temperature range of above 125 deg C or above).
Note: "…
Part Number: SN65LVDS822 Hi,
as we are using the following parts in one of our design, so I request you to please share the availability and longevity for the same.
1. SN65LVDS822
2. THS8200IPFPEP
3. TVP6000
Regards,
Sanjay
Part Number: SN65LVDS822 Other Parts Discussed in Thread: SN65LVDS93A Hello, My customer would like to connect SN65LVDS93A inputs to SN65LVDS822 outputs.
The following connections are correct? If not, please show the correct connections SN65LVDS93A inputs…
Part Number: SN65LVDS822
Hi, Support Team
SN65LVDS822 is can support LVDS to RGB888 of frequency 8MHz
also we need as below inquire can support minimum freq 8MHz, Automotive parts is better.
Q1: LVDS to MIPI CSI
Q2: LVDS to CSI
Q3: RGB888 to MIPI CS…
Part Number: SN65LVDS822 Other Parts Discussed in Thread: SN65LVDS93B
Team,
I cannot find the SN65LVDS822RGZEVM board listed on TI.COM. -Has it been discontinued? -Could we make the GERBER file available so that customer could build it and use samples to…
Part Number: SN65LVDS822 Other Parts Discussed in Thread: DS90CF364A , DS90CF384A
Hi Team,
Can SN65LVDS822 support RGB666? Do supporting 18 bits color mean that it can support RGB666? Is there any low cost devices that support 18bit RGB, HSYNC, VSYNC…
Part Number: SN65LVDS822 Other Parts Discussed in Thread: DS90CR286AT-Q1 , DS90CR286A-Q1 , SN65LVDS86A-Q1 Hi all
My customer has a design with the SN65LVDS822.
Because of the constrained market they are looking for a potential replacement option.
Is there…
Part Number: SN65LVDS822 Hi team,
I have an inquiry from my customer.
1. They have a 5" TFT LCD, 800x480 resolution, with 24 bit RGB interface + capacitive touch panel (I2C). The screen is used for HMI, so there are no "heavy" video requirements.…