Part Number: SN65LVDS86A Other Parts Discussed in Thread: SN75LVDS82 , Hi,
Is there have SN65LVDS86A reference design can provide to me?
My customer want to change LVDS solution from SN75LVDS82 to SN65LVDS86A,
They wants to know there have big change and reference…
Part Number: SN65LVDS822 Other Parts Discussed in Thread: SN65LVDS86A Hi,
Greetings.
Looking for the following part in "SN65LVDS822" in Automotive or Military grade (having operating temperature range of above 125 deg C or above).
Note: "…
Part Number: SN65LVDS86A Hello team, My customer checked the receiver input skew margin of SN65LVDS86A at almost 65MHz clock as below.
But they requested me to confirm the performance of the receiver input skew margin at 35MHz clock because they think that…
Other Parts Discussed in Thread: SN65LVDS86A-Q1 Hi Champs,
My customer asked about PCB pattern layout of SN65LVDS86A-Q1, especially pattern layout around VCC and GND
Can you please provide it?
Best regards,
Nobuo Fujihara
Other Parts Discussed in Thread: SN65LVDS86A , DS90UR906Q-Q1 Dear Team.
I'd like to know which value SN65LVDS86A has for 'Deserializer delay' .
For example, DS90UR906Q-Q1 has the specifiation of 'Des delay' as below.
(tDD=Deserializer Delay…
Part Number: SN65LVDS822 Other Parts Discussed in Thread: DS90CR286AT-Q1 , DS90CR286A-Q1 , SN65LVDS86A-Q1 Hi all
My customer has a design with the SN65LVDS822.
Because of the constrained market they are looking for a potential replacement option.
Is there…
Based on the datasheet, TI is supporting SXGA (1280x1024). If we
are looking at the specs, the max clk speed is 68MHz including the Vertical &
Horizontal ratio blanking. What is the refresh rate at this speed? Can we reach
60Hz @ full resolution? Thanks…
Part Number: SN65LVDS84AQ-Q1 Other Parts Discussed in Thread: SN65LVDS86A
My application requires <10us latency distribution of a 128-bit signal over 10m of CAT6e. Needs to support 100C .
Based on my browsing I'm planning to use the combination 6 …