LVDS Unlock Issue FA Report-20221114.pdf
Hello Josh
Thanks for your comments.
Finally we found the cause is R41 resistance various from 47 ohm~2K ohm, some of R41 resistor value even open.
visual check we found R41 is damaged, checked with Vendor R41…
Part Number: SN65LVDT2 Hi Team,
My customer needs clarifications regarding the two ICs, please see details below.
I am looking for a replacement for the SN65LVDT2DBV LVDS receiver IC in the SOT23-5 package with the internal 100 Ohm resistor. T he DS90LT012AQMFX…
Part Number: SN65LVDT2 Other Parts Discussed in Thread: DS90LT012AQ-Q1 , SN65LVDS2 , DS90LT012A , DS90LV012A Hi Team,
Can you suggest an alternative for SN65LVDT2? I found SN65LVDS2 however, the SOT23 package is out of stock. Is DS90LT012AQ-Q1 a good alternative…
Part Number: SN65LVDT2 Hi Experts,
My customer is asking about VID(Differential Input voltage) spec for LVDS receiver. VID is specified as 1.0V max(abs max) and 0.6V max(recommended).
Looking at the receiver test condition, it uses 0.8V VID signal. …
Part Number: SN65LVDT2 Other Parts Discussed in Thread: SN65LVDS4 Hi
We are using SN65LVDT and LVDS in our design, for our reference clock distribution at 100MHz, recently our customer asked us for a lower Phase Noise Ref Clock, our new TCXO has good phase…
Part Number: SN65LVDT2 For SN65LVDT2, can you clarify loading on the receiver outputs?
In Figure 3 and Figure 4 of the DS, it appears we can safely apply various loads to the output and allow for safe operation.
However, if the datasheet, abs max for receiver…
Part Number: SN65LVDT2 There appears to be an error in one of the tables in the datashseet. In the pinout table on p4, the description for the LVDS pins lists them as outputs, but they are actually inputs on the receiver. It seems like a copy-paste error…
Part Number: SN65LVDT2
Hi All,
Hope you are well. I have a question about the SN65LVDT2DBVT. The transceiver is used on a current design where the differential input clock is a 125MHz, 3.3 LVCMOS signal. The VCC of this transceiver is at 3.3V as well.…
Part Number: DS90LV012A Other Parts Discussed in Thread: DS90LT012A , SN65LVDT2 Hi Team,
Are these devices drop-in compatible with each other?
Thank you,
Franz