Part Number: SN65MLVD201 What is the junction limit for SN65MLVD201DG4? The only information in the datasheet is that the operating temperature is 85°C and the max storage temperature is 150°C.
Hi ElecFun,
Apologies for delay in response,
We suggest to use AM243x can support such interface. It has a co processor called PRU ICSSG. There is hardware support for PRU to do serial2parallel conversion in RX and parallel2serial conversion on TX. See…
Part Number: SN65MLVD201 Hi,
We are planning to use SN65MLVD201DR based half duplex link between two boards using 100ft of shielded cat5e cable, and wondering if even possible to achieve 100Mbps of data rate using 8b/10b encoding scheme. I found signaling…
Part Number: SN65MLVD201 Hi Expert,
Using MLVDS - SN65MLVD201D, we have question about this part regarding the Failsafe biasing of MLVDS. We want to ensure that customer are following the information in the data sheet to choose the resistors.
R3 = ~ 5kohm…
Part Number: SN65MLVD201 Hello,
I am testing a device which is using an M-LVDS driver to replace an RS485 driver to achieve better performances... the driver is the SN65MLVD201, and I have a trasmitter sending data by UART through the driver on the bus…
Part Number: SN65MLVD201 I’m looking for some additional information on one of your M-LVDS drivers (SN65MLVD201). I’m specifically trying to determine if the differential IO (A and B) remain high-impedance (can tolerate the line being externally…
Other Parts Discussed in Thread: MLVD20XEVM , SN65MLVD201 , THVD1450 , SN65LVDS050 Hi TI,
Newer engineer here, I have a 1PPS signal that will be provided via LVDS signal standard but is required to be sent to the receiver as a RS-422 compliant signal. Does…
Part Number: SN65MLVD201 Other Parts Discussed in Thread: P82B96 Hi Team,
A customer's project needs a two-way io board to board transmission, about 1M speed. Customer would like to know can the differential drive be used like this?
Thanks,
Annie …
Part Number: SN65MLVD201 Hi,
I am looking for the following thermal information for the SN65MLVD201 Component.
Thermal resistance from junction to case top - Theta JC
Thermal resistance from junction to case bottom - Theta JC
Thermal resistance from junction…