Part Number: SN74AHC00 hello,
could anyone please confirm or correct rather suspicious pinout in https://www.ti.com/lit/ds/symlink/sn74ahc00.pdf?ts=1708329446400
It substantially differs from standard 7400 pinout layout
regards
JS
Part Number: SN74AHC00 Hi,
I am looking for a logic family (inverter or buffer) which can toggle at 100MHz.
Which TI logic family is most suitable for this speed? Is AHC still the fastest logic family that TI offers or is there a faster option?
Part Number: SN74AHC00 Per Material Declaration , The Bond wire is copper, Need a Copper wire Qualification Test Report (Test performed on WIre bond , Wire Shear test) per AEC , but when i ask a Query i get a SGS Report, but that report doesnt specify…
Part Number: SN74AHC00
I am considering the following two products.
SN74AHC00PWR
SN74AHC02PWR
Which of the following are reliability test data?
AC or UHAST
THB or HAST
Part Number: SN74AHC00-Q1 Hello ,
I am looking for some informations regading the process FAB Technology of the SN74AHC00-Q1 :
-The Mask SET / The die Revision . -How we can get easily the FAB Site / The Diffusion Lot /the Wafer N°
Those requested datas…
Part Number: SN74AHC00-EP Hello ,
I am looking for the TI full Reliability Report for SN74AHC00MPWREP as this email link thasn't work or probably doesn't exist .
Thank you in advance for your support .
Best regards .
All devices with TTL-compatible inputs require a nominal 5 V supply. That 2 V – 5.5 V voltage range would apply to the SN74AHC00. (And the drive strength of 8 mA is not higher than that of the AC device.)
Part Number: SN74AHC00 Hi Team,
Could you tell me how to deal with Power pad land? Fundamentally, power pad land should be connected to GND, but there is no description in the datasheet.
Regards,
Takashi Onawa