Part Number: SN74AHC1G125 Hello guys,
One of my customers is evaluating SN74AHC1G125 for their new products.
They connect a few LC filter and a pull down resistor to Y output of the device. Also they input 16MHz signal to A input. At this moment, they have…
Part Number: SN74AHC1G125 What is the input impedance, or input current, on the OE# pin of the SN74AHC1G125? The datasheet seems to imply this is a +/- 1uA, but the PSPICE model shows a 2000 ohm impedance to GND. Is this just an error in the spice model…
Part Number: SN74AHC1G125 Hi all,
At what point would you use a digital buffer like SN74AHC1G125 for buffering digital signals to improve noise integrity over a long distance (like 1ft) vs something like a RS-422 or RS-485 differential line transceiver…
Part Number: SN74AHC1G125 Other Parts Discussed in Thread: TXU0101 , TLV7011 Hi Team,
My customer needs a buffer device which has higher V IL threshold compared to the SN74AHC1G125. They're looking for 1.8V at Vcc = 3.3V. Is there any device with this specification…
Part Number: SN74AHC1G125 Hi, Staff
Is it possible to provide the IBIS Model of SN74AHC1G125DC? There seems to be no IBIS Model on the product homepage.
best regards cafain
Part Number: SN74AHC1G125 Hello team,
Are there any limitation for output capacitor ?
Our customer will put the capacitor at 0.1uF – 1.0uF of 5V.
The background is that customer would like to implement RC circuit and concerned if a resistor is…
Part Number: SN74AHC1G125 Other Parts Discussed in Thread: SN74LVC1G123 Hi,
The reset pulse will cause the input to go low briefly at the end of the pulse input.
what kind of protection circuits this device has. Normally the two diodes at the input protect…
Part Number: SN74AHC1G125 Hi Team,
May I ask whether SN74AHC1G125 passes the UL certification? If yes, could you offer the UL number or some UL statement?
Thanks!
Part Number: SN74AHC1G125 Hi team,
Could you provide me the junction temperature Tj value of SN74AHC1G125? We didn't find from the datasheet.
Regards,
Yoshi