Part Number: SN74AHCT00Q-Q1 Hello,
This might be an FMEA-related question, but does the SN74AHCT00QPWRQ1 have a failure mode that causes its outputs (pin 3, 6, 8, and 11) to stick to High?
Best regards, Shinichi Yokota
Part Number: SN74AHCT00Q-Q1 Hi,
I am checking the VOH of SN74AHCT00Q-Q1. I have two questions. (1) There are specifications when IOH = -50uA and -8mA. What is the VOH for -600 uA? Is there a calculation method? (2) VOH is specified with VCC = 4.5 V. When VCC…
Part Number: SN74AHCT00Q-Q1 Hi,
I am checking whether the IC may not operate properly depending on the instant of power supply interruption time and the value of power supply voltage. The figure below is an image. Are there any conditions that cause problems…
Part Number: SN74AHCT00Q-Q1 Hi
Our customer is requesting data about current consumption (min, typ, max) of SN74AHCT00Q-Q1.
Do you have it?
BestRegards
Chris,
The end application is an automotive product. So, I guess the question is linked to FMEA. I believe it's not that an issue is happening now.
I asked the same question about another product, SN74AHCT00Q-Q1, and the answer says a damage to the…