Part Number: SN74AHCT1G04 Hello
We would appreciate it if you could provide us datasheets of SN74AHCT1G04DCKR for Rev.N, RevO, and RevP.
Also, if you have issued PCNs for each Rev, we would appreciate it if you could also provide us related PCNs.
Thank…
Part Number: SN74AHCT1G04 Dear Experts,
We would like to know Maximum ratings of ESD as MM model for SN74AHCT1G04DCKR.
Our customer ask us it. Would you kindly tell us?
Best regards,
Yusuke Kawate
TED
Part Number: SN74AHCT1G04 Hello, I am trying to simulate the behaviour on PSpice. I am providing 0-3.3V pulse input but it does not invert properly. It always gives a high input. Could you please help me with this issue? According to data sheet it should…
Part Number: SN74AHCT1G04 Dear
when using an active crystal oscillator to output an 3.3V Sinewave, we want to change the 3.3V Sinewave to 5V sinewave.
Is it OK to use a Inverting buffer/driver like SN74AHCT1G04 with 5V Power supply, 3.3V Sinewave input…
Part Number: SN74AHCT1G04 Hi,
Good Day. I have a customer who is working with SN74AHCT1G04. Please see his query below for your reference. Thank you very much.
Customer needs the values of overshoot max, undershoot max, rise & fall time, duty cycle, voltage…
Part Number: SN74AHCT1G04 Just wanted to confirm SN74AHCT1G04DCKR and 74AHCT1G04DCKRG4 are identical. They share the same data sheet, so I assume they are.
Regards, Mark
Part Number: SN74AHCT1G04 Other Parts Discussed in Thread: STRIKE My customer found a logic problem(SN74AHCT1G04DBVR) on existing products of motor driver.
Application: servo Motor
Sub-System: Inverter Logic for IGBT Braking application.
Problem: When…
Hi
The min of VIH is 2V.
I wonder this device can accept 2.5Vpp input signal. Is that possible?
(On the datasheet it is mentioned as the following,
The input switching levels have been lowered to accommodate TTL inputs of 0.8 V VILand 2 V VIH. This feature…
I would like to know if it is possible to to use the stated inverter gate at a supply voltage of +3.3V.
Obviously the data sheet indicates a supply voltage range of 4.5 to 5.5V, but is the part operational at a reduced voltage of +3.3V. It appears to…