Part Number: SN74ALS1034 Other Parts Discussed in Thread: CD74HC4050 , SN7400 Hi,
I am using SN74ALS1034 for buff drive. It is becoming obsolete?
Can you recommend me any alternative with temperature range from -40C to 85C?
Thanks,
Christie
So the LVC07 can not be used due to input logic!
It looks the SN74ALS1034 has no SOIC with higher temp of -40 to 85degree/105degree? Correct?
Customer need p2p compatible for 2nd source solution. please advice. thanks.
Regards
Brian W
There are two old bipolar devices with the same pinout, SN74AS1034A and SN74ALS1034. If the circuit runs at 5 V and can tolerate the higher input and supply currents, they are likely to work.