Part Number: SN74AUC1G08 Other Parts Discussed in Thread: SN74LVC1G08 Hello Team,
the SN74AUC1G08 can operate as abs. max at 3.6V while the maximum recommended voltage is 2.7V.
I'm not expecting any problem by operating the part by 3.3V continuous.…
Part Number: SN74AUC1G08 Other Parts Discussed in Thread: SN74AUP1G97 Hi Team,
Do we have solutions to achieve VIL_max>0.7V, VIH_min<1.2V, output high level up to 2.3V?
thanks a lot.
Yang
Part Number: SN74AUC1G08 Hi there,
I'm looking for a high bandwidth AND gate which can generate 1ns width pulse. I saw the tpd=tplh=tphl is 2ns for SN74AUC1G08 with CL=15pF. Do we have any device which is faster?
Thanks.
Part Number: SN74AUC1G08 Hi,
Now the customer evaluate SN74AUC1G08 by using its IBIS model, then they found strange VI characteristics at Pulldown and Pullup of AUC1G08_OUT_18 as attached. We usually see the linear VI characteristic but this does not has…
Part Number: SN74AUC1G08 The data sheet defines the probagation delay tpd but does not define the rise and fall times (10-90%)..
In particular, what are the rise and fall times when Vcc = 1.8V?
Thanks, John Garrett TI-AFA
Other Parts Discussed in Thread: SN74AUC1G08 , SN74LVC1G08 I build a simple circuit with SN74AUC1G08 IBIS mode, just as bellowed. The simulation soft is Hyperlynx.
The waveform at R4(Blue) and R5(purple) is captured as followed.
The signal by simulation…
Other Parts Discussed in Thread: SN74AUC1G08 I get the max frequency is 250MHz for SN74AUC1G08 from the parameter page.
When I use a signal of 100MHz for A and B, I found that the Y output of the device is correct.
When I use a signal of 200MHz for A and…
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74LVC1G08 , SN74AUC1G08 Hi Team,
My customer is asking is there's any description in d/s or info about output pin Y(pin 4)'s sink current data ?
I had check with d/s, not sure if IOH mean…
Hi,
Many of our logic devices will be able to handle 1MHz or above. Our logic gates don't have a frequency written in their datasheet but our flip flops do.
One example is the SN74AUC1G74. It can handle up to 275MHz. If you want the AND gate in this…