Hi Albert Xu1,
Please tell me the current status.
Since our customer's delivery deadline is fast approaching, we would like to receive a response from you as soon as possible.
Best regards,
Yutaro Hayashi
Part Number: SN74AUP1G08
Dear, Support Team.
Our customer asked about the weight of the SN74AUP1G08DCKR. I've been looking into it, but the PACKAGE OUTLINE in the data sheet did not include the weight. In addition, I looked at the TOTAL weight of Amount…
Part Number: SN74AUP1G08 We are looking for the θ_jc (°C/W), θ_jb (°C/W), and Max Junction Temperature (°C) for part numbers: MSP430F2274MRHATEP TCA9539RTWR SN74AUP1G08DCKR SN74LVC1G08DCKR
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74LVC1G08 , SN74LVC1G99 Hello TI experts,
My customer wants to apply different voltages to each input with SN74AUP1G08.
input B (pin1) : 4.0V
input A (pin2) : 1.8V
VCC : 1.8V
maybe output would…
Part Number: SN74AUP1G08 Hello expert,
My customer would like to double check with below issue in SN74AUP1G08 input voltage level. We applied 3.3V as VCC and raise two inputs to high. The level for VIH minimum is 2V but it seems like output turns high…
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74HCS08 , SN74AUP1G97 , SN74LVC1G97 Hello expert,
In [FAQ] How does a slow or floating input affect a CMOS device?, it mentions there is oscillation w hen the input lingers near the threshold value…
Part Number: SN74AUP1G08 Hi team, I can not find package information for SN74AUP1G08DRYR (SON (DRY) | 6). Could you tell me about "PACKAGE OUTLINE","EXAMPLE BOARD LAYOUT","EXAMPLE STENCIL DESIGN" ? Sincerely. Kengo.