Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 Dear Team,
Do we have any solution without internal pull high and can P2P replace 74AVCH1T45GW?
Many Thanks,
Jimmy
Part Number: SN74AVC1T45 Hi Team,
For SI analysis, we are in need of S-parameter for the part SN74AVC1T45DBVR. We can't able to find the S-parameter of that part at ti.com.
Where we can get the S-parameter for that part?
Thanks in advance.
Part Number: SN74AVC1T45 Dear TI support Team,
We are using the SN74AVC1T45 in our design and have accidentally referred the voltage on the DIR pin to VCCB instead of VCCA.
Design setup: VCCA = 1.8V, VCCB = 3.3V and DIR pin is tied to 3.3V.
According…
Part Number: SN74AVCH1T45 Other Parts Discussed in Thread: SN74AVC1T45 , SN74AUC1G17 , 2N7001T , SN74AUP1G17 , SN74AUP1T34 , TXU0101 , SN74LVC1G17 I am planning to use SN74AVC1T45 and SN74AVCH1T45 to level shift 25MHz clocks. An example circuit in our application…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 We use a SN74AVC1T45DCKR for a signal level shift. But we find our product only provide v1.05v for VCCA, it doesn't satisfy minimum operation voltage 1.2V that is descripted in datasheet…
Part Number: SN74AVC1T45 Can you tell me the max junction temperature for SN74AVC1T45DCKT
A max storage temperature is given at 150C in the datasheet but not a max operating TJ. Is it also 150C?
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 , TXU0101 , TXU0102 Dear Team,
Could you help to do level shift schematic review?
MPN: SN74AVC1T45
Direction: A->B
IPQ_GPIO27 and IPQ_GPIO28 connect to CPU GPIOs directly.
Many Thanks…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 Dear All,
Looking for the Voh and Vol values since the datasheet doesn't mention these. Please help.
Thanks,
Saurabh
Part Number: SN74AVC1T45 customer application shows VCCa and VCCb connected to the same power supply.
according to data sheet, power supply considerations are as follows:
1) Connect ground before any supply voltage is applied. 2. Power up VCCA. 3. VCCB…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 Hi TI teams,
For SN74AVC1T45, I deployed below design and there is a pull down resistor on port B. In the design, VCCA will be powered up first, and we observe a glitch on port A when…