Part Number: SN74AVC4T245-Q1 Other Parts Discussed in Thread: SN74AXC4T245-Q1 Hi team,
Could you provide a comparison between the SN74AVC4T245-Q1 and the SN74AXC4T245-Q1?
Are they able to use a 1kΩ pull-down resistor on the output side?
Thank…
Part Number: SN74AVC4T245 Hello.
Another board provided a 66.67MHz 1.8V LVCMOS clock through cables. Now I need to convert to 3.3V LVCMOS for CPLD as the system clock. Is SN74AVC4T245RSVR OK?
Part Number: SN74AVC4T245 Other Parts Discussed in Thread: SN74AXCH4T245 , SN74AVCH4T245 Team,
I want to check with you if SN74AVC4T245RSVR supports BUS Hold function? Thanks!
BR
Qiang
Part Number: SN74AVC4T245 Other Parts Discussed in Thread: AFE8190 Hi Logic team,
I am Taemin who is FAE support Samsung NW in Korea.
My customer designed SN74AVC4T245 as level shifter between USB(3.3V) and AFE(1.8V).
I removed pull-up path at the SPIA…
Part Number: SN74AVC4T245-Q1 Other Parts Discussed in Thread: SN74AVC4T245 Dear TI support team,
Our SN74AVC4T245-Q1 schematic is as follows,
On one board, after I remove R3 and R6( that means the input pin and out pin are floating), the voltage of pin…
Part Number: SN74AVC4T245 Other Parts Discussed in Thread: SN74AVC2T245 Team,
I'm confused about SN74AVC2T245 datasheet as below, can you help me with it? Thanks!
What's Vtp? Why we should have Vtp considered when calculating Tplz and Tphz?
…
Part Number: SN74AVC4T245 Hi team,
My customer want to use our SN74AVC4T245RGYR.
And the typical circuit is as below:
Customer have five questions:
1 、If they connect 1OE 、 2OE 、 1DIR to 1.2V, 2OE to GND, and choose SN74AVC4T245RGYR 1A data to 1B data,2B data…
Other Parts Discussed in Thread: SN74AVC2T245 , SN74AVC4T245 , SN74AXC4T245 , SN74AXC2T245 Team,
Customer is looking for a similar TI products compared to our SN74AVC4T245 and SN74AVC2T245.
Preferred same package and pin define as UQFN | 10. But Vcc could…