Part Number: SN74AVCH8T245 Hello Team,
is it ok to connect unused ports directly to ground or do you have a better recommendation, please?
Thanks and Best Regards, Hans
Part Number: SN74AVCH8T245 Hi team,
Customer is trying to use the device as level shifter and the communication speed is about 100MHz and bi-directional. So DIR-pin needs be Low/High.
Then, they want to understand the switching characteristics of DIR…
Part Number: SN74AVCH8T245
Why is the switching time from high to low ( rise/fall time) increase with decrease in Voltage levels?
At 5V the switching time is less and at 1.8V the switching time is increased.
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , SN74AXCH8T245 Dear Sir,
Have you an explanation regarding huge propagation delay dispersion from 0.5 ns which is minimum up to 4.4 ns which is maximum? for SN74AVCH8T245 device…
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AXCH8T245 Hello,
Regarding SN74AVCH8T245:
Thermal PAD at PACKAGE OUTLINE(page 28) have number 21 .
Termal PAD at EXAMPLE BOARD LAYOUT(page 29) have number 25 .
Termal PAD have number 25 and…
Part Number: SN74AVCH8T245 There is a very detailed Tpd table on the datasheet.
It gives max and min prop times
Is there a guidance on what the gate to gate Tpd variations are?
Is it possible to max one at max and one at min delay? I realize that's extreme…
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , SN74AXCH8T245 Hi,I am currently working on a project that uses SN74AVCH8T245DGVR.The datasheet of the SN74AVCH8T245 does not provide the information about the package drawing of DGV…
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AXCH8T245 , Hi Team:
Could you offer TPLH / TPHL MIN & MAX value to me ? Thx.
When VCCB is 3.3V.
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AVCH4T245 Hello,
IBIS model in TI.com provide IBIS for TSSOP and TVSOP packages.
I need model for QFN.
How can I get it?
thank you,
Ofer.