Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74LVC1G3157 , TS5A63157 , SN74LVC2G53 Hi,
We are using SN74AXCH8T245PWR in our design to convert 25MHz signal from 3.3V to 0.75V. When we got the board and test it, we see that this part is not…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 I designed a circuit using the Telit GE190C1-EUX GSM modem. Since the GSM side operates at a 1V8 voltage level and my processor operates at a 3V3 level, I used the SN74AXCH8T245…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: TXV0106-Q1 , SN74AUC34 , TXV0108-Q1 Hi,
Does SN74AXCH8T245 suitable for below application?
We need to use it for the signals on Ethernet MAC GMII. 1.5V to 1.8V (1.8V to 1.5V). The signals include…
Part Number: SN74AXCH8T245 I need to translate a 1.8V, 5ns pulse to 3.3V. Will the SN74AXCH8T245 work? If not does TI have a better solution?
Thanks,
Kevin
Part Number: SN74AXCH8T245 I am looking for the level translator between 3.3V and 1.2V (uni or bi-direction) at >200Mbps. Does SN74AXCH8T245 meet this requirement? (cannot see speed rate at 1.2V from the datasheet). If not can you recommend one?
Thanks…
Part Number: SN74AXCH8T245 Hi Team
my customer is using SN74AXCH8T245RHLR, VCCA = 1.8V, VCCB = 3.6V, I saw your publications Glitch free power sequencing with AXC level translators (Rev. A) (ti.com) ,
1) As the power-up hi-Z circuit is before the output…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , SN74AVC8T245 Hello,
Our customer is experiencing the RGMII issue when using SN74AXCH8T245 as level shifter from 1,8V FPGA to 3.3V PHY (for both TX_CLK and all TX_DATA). Specifically…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AVC8T245 , SN74AXC8T245 , Hi Team,
Issue background: 1.8v -3.3v translation RGMII buffer which works well at 100Mbps but fail at the 1000Mbps wi th part SN74AVC8T245 . Now we are question ab…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , , SN74AVCH8T245 Dear Sir:
The current system uses SN74AXC8T245 as the I2S&SPDIF buffer.
Because SN74AXC8T245 is out of stock recently, can I use SN74AXCH8T245 instead?
Best…
Part Number: SN74AXCH8T245SN74AXCH8T245PWR is out of stock, and replace it with SN74LVH8T245PWR. The maximum working temperature of SN74AXCH8T245PWR is 125℃, but the maximum working temperature is 85℃. The board temperature of customer is 90℃. If over…