Part Number: SN74CB3Q3245 Hello team,
Datasheet says NC is no internal connection, so should I connect NC pin to GND or leave it floating?
Also should I connect thermal pad to GND?
Best Regards, Kei Kuwahara
Part Number: SN74CB3Q3245 Other Parts Discussed in Thread: SN74CB3T3245 Hi team, I'd like to ask about the difference in output characteristics between SN74CB3Q3245 and SN74CB3T3245. Below is the conditions under which I want it to work. VCC = 3.3V Vin…
Part Number: SN74CB3Q3245 Hi Team,
The customer found that the IO model of SN74CB3Q3245 cannot be set as output, why? Could you pls help?
Regards, Hailiang
Part Number: SN74CB3Q3245 Hi there,
can you please provide below data to my customers?
Q1: θ jc=? Q2:Max withstanding operating junction temperature spec Tj=?
Part Number: SN74CB3Q3245 Hi Experts,
Good day.
We would like to ask assistance to provide the following missing parameters for the part SN74CB3Q3245RGYR:
Q1: θjc=? Q2: Max withstanding operating junction temperature spec Tj=?
Thank you.
Regards, …
Part Number: SN74CB3Q3245 Other Parts Discussed in Thread: SN74CB3Q3125 Hi Team,
I got a request from a customer, that in the IBIS model for SN74CB3Q3245 the pins can only be configured as inputs but not as outputs even though they are bidirectional. …
Part Number: SN74CB3Q3245 Dears
Could we keep the device AX and BX floating? The device have 8 I/O, but we only need 6. So we need your suggestion about how to take care of the used pin?
Thanks
Jun Shen
Part Number: SN74CB3Q3245 Hi there,
My customer used SN74CB3Q3245 for signal swtich. They are confused with 'Latch-up performance'. So could you give me an explanation about this function?
I can't find related contents in our datasheet.
Best…
Part Number: SN74CB3Q3245 Other Parts Discussed in Thread: TMUX1511 Hi,
Please suggest if we can use SN74CB3Q3245 part for the attached NCSI interface use case.
The Enable signal doesn't switches from 0 to 1 only once.
REF_CLK Frequency
50…
Part Number: SN74CB3Q3245 Hi,
could you recommend a other device that P2P with SN74CB3Q3245 and the bandwidth is about 200MHz.
I find the SN74CBT3245, but the VCC is 5V . customer need 3.3V supply.
thanks in advance.