Part Number: SN74CB3Q3257 Tool/software: Hi, Can SN74CB3Q3257PWR E4 be substituted for the SN74CB3Q3257PWR? I see an old datasheet (2009) with reference to the “E4” version, but it doesn’t list why it is different. Thanks!
Part Number: SN74CB3Q3257 Tool/software: I am concerned about device heat generation when passing a 50MHz CLK. Is there any difference in heat generation when passing signals below 1kHz? I would appreciate any calculation formulas or reference information…
Part Number: SN74CB3Q3257 Other Parts Discussed in Thread: SN74LVC1G66 , , SN74AVC4T774 Tool/software:
We used two parts on SPI bus, SN74CB3Q3257 has CLK/CS/IO1/IO2 and SN74LVC1G66 has IO3/IO4.
Propagation delay is MAX 0.8 ns on SN74LVC1G66,Propagation…
Part Number: SN74CB3Q3257 Tool/software: Hi TI:
I need to read 8 resistive dividers with a MSP432. I only have available 4 analog pins of the MSP432, I plan to multiplex through a SN74CB3Q3257PWR according to the attached schematic.
However in a proteus…
Part Number: SN74CB3Q3257 Other Parts Discussed in Thread: LM339 , Hello,
Some TI devices, such as LM339, give a maximum "case temperature" spec in the datasheet. I do not see an equivalent spec for SN74CB3Q3257. Can you please let me know the maximum…
Part Number: SN74CB3Q3257 Other Parts Discussed in Thread: SN74CBTLV3257 Hi team,
I have a concern about the SN74CB3Q3257 IO signal level, I want to use this IC’s IO for P1V8 JTAG signals select, according to the datasheet, it should be ok when VCC…
Part Number: SN74CB3Q3257 Other Parts Discussed in Thread: TMUX1574 Can you please share the details of channel to channel crosstalk, off isolation and -3dB bandwidth of the IC (SN74CB3Q3257DBQR).
Maximum voltage and current rating for hot insertion…
Part Number: SN74CB3Q3257 Hello, Team
May I know if our SN74CB3Q3257 pin A1/A2/A3/A4 has a build-in pull up resistor?
and what`s is the parasitic capacitance on A1/A2/A3/A4 pin?
Part Number: SN74CB3Q3257 Hi Team,
Customer report that when they test the waveform at control input pin (OE, S), The low voltage is -0.08V, which exceeds the recommended operating voltage VIL. Are there any risks?
Regards, Haiiang
Part Number: SN74CB3Q3257 Hi TI,
Please provide the reliability parameters of SN74CB3Q3257: MTBF, reliability (Rt), failure rate (λ). Are all the part numbers the same? Or are there different situations for different part numbers? Br Cayden