Part Number: SN74CBT3125C Hi team,
My customer would like to know the temperature spec.
Do we have the Tc_max (case temperature) or θjc spec for SN74CBT3125CRGYR?
The reference information that is not guaranteed is also helpful.
Best regards,
Yu…
Part Number: SN74CBT3125C Hi
I use the device as test driver and then there's question about "ON-state switch current, II/O ±128mA " for 4 output port sharing.
When only active one output port (ie. 1B ON but 2B/3B/4B OFF), dose driving…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: SN74CBT3257C , SN74CBT3125 Hello,
My customer is evaluating use of 2x SN74CBT3125C in place of SN74CBT3257C due to space constraints.
Is the switching frequency between these two parts the same…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: TMUX1511 , TMUX1574 , Hi,
I am looking for a smaller SPI level shift solution. The application include a "motor driver” that communicates with “host controller”. SPI voltage for driver is 3.3V while…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: TMUX1511 Hello,
It seems I've made a mistake by powering the SN74CBT3125C with a 3.3V supply in my design. It's been working so far, but what operating parameters are limited at lower VDD?…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: SN74LVC1G139 , TS12A44514 , TS12A44515 , TS12A44513 Hi All,
I have a question about SN74CBT3125C.
Is 1B output when VCC and 1A are shorted? When a voltage of VCC-0.8V or more is input to 1A, is the…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: TMUX1511 Can you please confirm that SN74CBT3125C is suitable to use with I2C signals? The master is on the A side and slave is on the B side. SDA and SCL /OEs are turned on at the same time.
…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: SN74CBT3125C , , TMUX1133 , TS12A4516 E2E,
Could devices like the SN74CBT3125C or SN74LVC1G3157 have something like -2.5V at GND and 2.5V at VCC and operate normally? I need to pass a -2.5V to…
Part Number: SN74CBT3125C Other Parts Discussed in Thread: TS12A44514
Hi,
I have been using this switch and I have been noticing a 1V drop across the IC and I am not sure why this is happening. First I thought I was experiencing some loading issue, but…