Part Number: SN74CBTLV1G125 Hi everyone,
I have a question about the switching on the SN74CBTLV1G125.
The datasheet states that when OE(pin 1) is pulled low, then A (pin 2) is connected to b (pin 4).
Is this a real switch?
The datasheet states that…
Part Number: SN74CBTLV1G125 Hi team,
Is there any difference between 74CBTLV1G125DCKRG4 and SN74CBTLV1G125DCKR?
and how to explain this--> "(6) Lead/Ball Finish - Orderable Devices may have multiple material finish options. Finish options are separated…
Part Number: SN74CBTLV1G125 Hi Support Team.
In the Qualification Summary, the results of ESD-HBM and CDM are described as "See data sheet". However, the datasheet does not show the results of ESD.
Please tell me ESD data (HBM data , CDM data…
Part Number: SN74CBTLV1G125 I need this device to operate in temperature region of -40 to +105C, but perferably 40 to +125C.
Is there and extended temperature or Automotive version of this device?
Thanks.
Part Number: SN74CBTLV1G125 Hi team,
Good day.
Our customer would like to know the HBM, CDM and MM ESD rating for the following devices:
SN74CBTLV1G125DCKR
SN74CBTLV3125DBQR
SN74CBTLV3251PWR
Thank you in advance for your help.
Regards, …
Part Number: SN74CB3T1G125 Other Parts Discussed in Thread: SN74CBTLV1G125 Hi,
We use CB3T1G125 throughout our design as a leakage prevention device instead of level shifting. Basically, we expect this part to be closed when there is power (3.3V) and open…
Part Number: SN74CBTLV1G125 Other Parts Discussed in Thread: TMUX1101 , TS5A3167 , Hi Team, we would like to ask the information of the ESD Rating and Class.
Thank you very much
Regards,
Mark
Part Number: SN74CBTLV1G125 Hi,
I have a question regarding this part,
The datasheet specifies a VinHighMin of 2V when supplied at 3V3.
We assume the A to B connection are 2 FET switches so it should not care about high or low as it is just an analogue…