Part Number: SN74CBTLV3253 Hi team,
1. There is no specific description of VIK, IL, Ioff and Icc parameters in the data manual. Can you explain it?
2. What does VIK=-1.2V mean?
3. Is the leakage current of 1uA for the whole chip rather than a single channel…
Part Number: SN74CBTLV3253 Hi Expert,
The engineer would like to know whether SN74CBTLV3253 can support the XSMI(15.6M) interface.
The XSMI has same performance as SMI interface (MDC / MDIO )
Only the speed different is SMI(1.95M) and XSMI (15.625M).The…
Part Number: SN74CBTLV3253 Hi ,
It is Jon from Inventec sever team.
Now we found the symptom need your support.
Our project use TI SN74CBTLV3253 and found some abnormal symptom.
As SPEC logic diagram below pig1,
When S1 = H (3.3V), S0 = L (0V), force…
Part Number: SN74CBTLV3253 Hi team,
could you please help to check the difference between SN74CBTLV3253PW and SN74CB3Q3253PWR?
Thanks, looking forward to your reply.
Part Number: SN74CBTLV3253 Other Parts Discussed in Thread: TMUX1136 , TMUX1119 Do you have 3.3-V, " 2:1 ", 2-channel analog multiplexer which supports Ioff function ? Thanks.
Part Number: SN74CBTLV3253 Other Parts Discussed in Thread: TMUX1209 Hi team,
My customer is using SN74CBTLV3253 and have some spec question to ask,
so quick check on the spec question of SN74CBTLV3253 ,
1. This device internally using FET as switch(“SW”)…
Part Number: SN74CBTLV3253 Hi,
On one our boards, we are using this switch to multiplex a logic signal. I had a question here. Can we float one of the selection pin (S1)?
I do not have the use of lower two channels (1B3 & 1B4), so I am just using S0 to…
Part Number: SN74CBTLV3253 Other Parts Discussed in Thread: SN74CB3Q3253 Hi team,
we want to check if the Vin voltage is higher than VCC, whether the Vin pin will source current to VCC? Thanks.