Part Number: SN74HC125 Other Parts Discussed in Thread: SN74HC244 I tried ti simulate a PCB design with CI buy I could not find the IBIS model and it is not available in TI web.....any ideas?
Hey Ibrahim,
Interesting strategy. It's more complicated than just using the driver's built in Mode 4 - Dual full bridges (one PWM input each full bridge). I'm not experienced with the SN74HC125, but I pulled up its datasheet and compared schematics…
Hi Christo,
As Nirav indicated, you may need to buffer TDO and TDI signals in the chain. For our case, we had to use SN74HC125 to buffer the signals. You also have to ensure that the trace length of the signal chain is kept at a minimum. I think the guidance…
Part Number: SN74LVC125A Other Parts Discussed in Thread: SN74HC125 , SN74AHC125 It looks like DIP package options are only available in 5V chips and not 3.3V. True?
Other Parts Discussed in Thread: SN74HC125 , SN74AHC125 , SN74S240 , SN74LVC244A , SN74LV541AT Hello,
I had a requirement where i need a 1:2 differential TTL IC.
My input is 100MHz differential TTL.
I need to have same signal that should be repeated twice…
Part Number: SN74LS125A Other Parts Discussed in Thread: SN74HC125
Dear Technical Support Team,
I have a question about SN74LS125AN.
I see overshoot on output pin.
■Q1
How is absolute min of output(Y)?
■Q2
Is this overshoot inside a permissible range on…
Other Parts Discussed in Thread: ADS8364 , SN74HC125 , 5-6KINTERFACE Hello,
I am very new to DSP hardware. I am trying to sample an analogue signal and store it on a computer. I am using the ADS8364EVM to do Analog-2-Digital conversion and the C6713DSK…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…