Part Number: SN74LV123A Hello team,
Could you please let me know about tPLH?
The value is not clearly specified in switching characteristics table.
Is it OK to use tpd value for tPLH and tPHL?
Regards,
Itoh
Part Number: SN74LV123A Hello Experts, My customer would like to design 1 sec timer by SN74LV123A. Customer tested the device almost 1 sec timer, using RT=100Kohm/CT=10uF. Customer got a good result but customer would like to know whether it is a reasonable…
Part Number: SN74LV123A Hi Team,
I have qustion about the SN74LV123AQPWRQ1.
Does this mean that when IOH (1Q, 2Q and its inverted output) is small, VOH is only guaranteed above 0.1V? Also, I am thinking of VCC = 5V. In that case, what will happen…
Part Number: SN74LV123A Other Parts Discussed in Thread: SN74LVC1G123 Hi guys, working with someone on this device (SN74LV123APWR), the datasheet wasn't clear.
If we are planning on using only half the outputs, so pins 5,9,10,12 are floating, how do…
Part Number: SN74LV123A Hello TI Forum,
I am trying to trigger the SN74LV123A on the rising and falling edge of the same signal.
For this I have shorted both inputs (inv&non-inv) of the same channel.
I works fine on ChA (white input to P1&P2…
Part Number: SN74LV123A Hello,
My customer made their own prototype with SN74LV123A. Then they found a wrong connection on Cext pin.
They wrongly connect this pin to GND directly like the below.
This is obviously different usage from the datasheet…
Part Number: SN74LV123A Hello team,
I received a question from my customer about behavior of monostable multivibrator logic "SN74LV123A".
Customers are willing to use VCC = 3.3V, and input voltage Vi = 5V(typ) for their application.
Vcc(3.3V)…
Part Number: SN74LV123A Hi,
I tried to simulate a circuit using SN74LV123A in orcad. The pspice model was downloaded from TI site.
I am using two multivibrator models in a circuit.
The first multivibrator consist of:
A high to low pulse given…
Part Number: SN74LV123A Hi Ti Sir
I have SN74LV123A Typical Application Problem. Pin Cext connect to GND. Is it correct ?
and Typical Application Cext do not connect to GND
Part Number: SN74LV123A Hello Team,
There is power-up ramp rate spec in our datasheet below, but there is only MIN spec. I think it should be MAX spec, what's your opinion? Why do we define this spec, if customer's application can't meet this spec,…