Part Number: SN74LV164A Other Parts Discussed in Thread: SN74AHC244 Hi TI team
Please refer attached Function Block Diagram, we used two TI logic IC, one is octal buffer and one is shifter logic IC.
Currently the U349 pin2 of input clock waveform whithout…
Part Number: SN74LV164A Hello guys,
One of my customers is using SN74LV164A for their mass production.
At this moment, they have the following questions. Could you please give me your reply?
Q. Recently, the device datasheet is modified from version SCLS403J…
Part Number: SN74LV164A Dear Sir/ Madam,
In SN74LV164ANSR datasheet spec, i can only find HBM and CDM model. May I know what is the MM(Machine Model) spec for this device?
ESD spec ESD Protection Exceeds JESD 22 ‐ 2000-V Human-Body Model (A114-A) ‐ 1000…
Part Number: SN74LV164A Dear Team,
Please confirm the below,
For the part No: SN74LV164APW, in datasheet at pin configuration for the pin 11 is mentioned as QF as output but in description for the same pin 11 is mentioned as QF and QH inverted.
Please…
Part Number: SN74LV164A Other Parts Discussed in Thread: SN74HCS164 Hello,
We are using the SN74LV164ADR in one of our design, and it seems like a perturbation is creating a strange behavior on the circuit.
In fact, when we have noise (inferior to 1V pp…
Part Number: SN74LV164A Hi,
I'm planning to use the VQFN version of the SN74LV164A. The datasheet states the thermal pad must be soldered to the PCB for mechanical and thermal performance. The datasheet further says the thermal pad should be connected…
Part Number: SN74LV164A Other Parts Discussed in Thread: SN74HC595 Hi Sirs,
Sorry to bother you.
Could you help double confirm our application as below?
We would like Serial to Parallel.
Schematic:
Part Number: SN74LV164A Dear Team,
Pls help to provide SN74LV164APWR “PD” & “TJ” information
PD: Maximum power dissipation
Tj: Maximum junction temp
BR
Kevin
Hi Tomasz,
You are not able call the product information API using a substring or wildcard search, but you are able to retrieve information for a "family" of products by using the GenericProductIdentifier query parameter.
If you call the product…
Part Number: SN74LV164A I have a number of devices I wish to obtain 'end of life' information, this is just one of them. Is there a better way to determine whether the devices are suitable for new design work? or can you comment on this particular device…