Part Number: SN74LV1T126-Q1 Other Parts Discussed in Thread: TXU0101-Q1 Hi team,
Under following condition, how much current consumption is when OE is low level?
V_cc=5.0V,
V_in=3.3 V
Best Regards,
Shoji
Part Number: SN74LV1T126 Other Parts Discussed in Thread: TXU0101 , In new buffer data sheet there is strange power consumption figure:
I don't understand what consumption this is. 0.3V is clearly "0" and 3.4V clearly "1". How come there is 1.35 mA consumption…
Part Number: SN74LV1T126 Team,
The previous version of SN74LV1T126 datasheet states that we will have an AECQ-100 spin soon. Can you advise whenever it would be available? Thanks.
Part Number: SN74LV1T126 Hi team,
I am looking for a 3 state buffer with below specs.
VCC is 1.8V – 3.6V
not Inverted OE
V_IH < 1.4V
package dimensions 2x2mm, H<1.1mm.
Do we have anything that fits better for those requirements than SN74LV1T126…
Other Parts Discussed in Thread: SN74LV1T126 Hello Clemens
Thanks a lot for your suggestion. If I use SN74LV1T126 and it is powered by 3.8V or even 5V, but the input signal could be 3.3V or 3V level(both OE and A), what is the supply current, could you…
Part Number: SN74LV1T126 Other Parts Discussed in Thread: SN74LVC1G126-Q1 , SN74AHCT1G126-Q1 , TXU0101-Q1 Team,
Would like to check if we have Q-grade spin for SN74LV1T126, or any similar alternative, to suit customer's automotive design that requires AEC…
Part Number: SN74LV1T126 Hi team,
What is the difference between SN74LV1T126DCKR and SN74LV1T126DCKRG4? Can SN74LV1T126DCKRG4 replace SN74LV1T126DCKR?
Thanks!
Regards,
Ivy
Part Number: SN74LV1T126 Other Parts Discussed in Thread: SN74LV4T125 Hello,
I didn't see an IOZ parameter on the SN74LV1T126 datasheet, how many is it? (The SN74LV4T125 datasheet says the IOZ is ±2.5uA (MAX))
Best regards, DDdoor