Part Number: SN74LVC08A Other Parts Discussed in Thread: SN74AUP1T08 , SN74HCS08 , TLV7011 the MCU output driect connect to SN74LVC08A input pin ,when the mcu init start ,there mcu has 1.5V square output , then the SN74LVC08A will have 1.5V square output…
Part Number: SN74LVC08A Hi Sir,
May I ask is there any input voltage requirement for SN74LVC08A to have Y pin output?
We using this SN74LVC08APWR IC for AND two PWM signal.
We found out that if the A/B input voltage about 2.4V, there will no Y output…
Part Number: SN74LVC08A Other Parts Discussed in Thread: ADS8920B , , SN74LVC1G17 , SN74LVC1G34 Hello,
Our customer is considering to use SN74LVC08A as a buffer to 50MHz SCLK input of ADS8920B. Can SN74LVC08A be used for this purpose? ADS8920B SCLK reqruies…
Part Number: SN74LVC08A Other Parts Discussed in Thread: SN74LV08A , Hi Team,
Could you please help with the below from a customer:
Device: SN74LV08ADR (2 Input AND Gate)
http://www.ti.com/lit/ds/symlink/sn74lv08a.pdf
What would the output state be when…
Part Number: SN74LVC08A I have a situation where the part might get 3.3V max to its input pins without power (Vcc = 0V). Will this damage the part in anyway? The datasheet seems to indicate the part will be fine, since the maximum voltage for Vin isn…
The SN74LVC08A-Q1 has different electrical characteristics (higher drive strength, I off ). But if you do not care about those, you can use the SN74LV4T08-Q1 instead.
Part Number: SN74LVC08A Hi team,
My customer asked if SN74LVC08A can support 1.8V power supply, in the datasheet, it said "Operate From 1.65 V to 3.6 V" in the first page, but in 7.3 Recommended Operating Conditions, it is 2V to 3.6V for operating…
Part Number: SN74LVC08A Hi team,
My customer is using the SN74LVC08A now, the input is over the datasheet spec(-0.5v) to -0.8v, whether it has risks here? Thanks.
Part Number: SN74LVC08A In my circuit this QFN-packaged IC is largely static, so I don't need the die-attached pad for thermal reasons. Do I need to solder it to a thermal pad on the PCB anyway? If so, should it be grounded or left floating? Thanks…
Part Number: SN74LVC1G07 Other Parts Discussed in Thread: SN74HCS21 , SN74HCS08 , SN74LVC08A Hi
I have a question about SN74LVC1G07.
VCC(3V3_PEX) voltage level with impact output (Y) voltage level?
If Tri_REG_PG use 3.3V is ok? thanks!
Jeff