Part Number: SN74LVC1G07 Hi TI,
So to be clear on the answered thread "e2e.ti.com/.../sn74lvc1g07-open-drain-output-pull-up-voltage-query
It should be okay to have a higher voltage on the output then is connected to VCC, as long as you not sinking…
Part Number: SN74LVC1G07 Do the DRY Thermal Metrics also apply to the DSF Package? I am looking for the DSF Junction-to-ambient thermal resistance, Junction-to-case (top) thermal resistance, and Junction-to-board thermal resistance. The data sheet reports…
Part Number: SN74LVC1G07 Hi,
This may not be a question particularly target to SN74LVC1G07. But it comes to me when I use the chip. When the part is un-powered, what's the output state I can expect? Hight impedance or low level?
Thanks.
Part Number: SN74LVC1G07 The difference between SN74LVC1G07DCK R & SN74LVC1G07DCK RE4 is the lead finish.
SN74xxxR is offered in both NIPDAU | SN
While SN74xxxRE4 is only offered in NIPDAU
Is the Matte Tin (SN) lead finish compatible with SAC 305…
Part Number: SN74LVC1G07-EP Hi Sir,
I use SN74LV1G07 to convert a 3.3V input signal to a 1.8V output signal.
However, due to the current design, the 1.8V power-up occurs before 3.3V, I'm not sure if there will be any abnormality in the output when there…
Part Number: SN74LVC1G07-Q1 Hi TI team,
We are using this buffer as a level shifter for reset signal from 3.3V to 1.8V .We are facing a problem while pulling the input pin to ground, but not getting the output fully low(it's getting low till 1.5V rather…
Part Number: SN74LVC1G07-Q1 Hi TI team,
We are using this buffer as a level shifter for reset signal from 3.3V to 1.8V .We are facing a problem while pulling the input pin to ground, but not getting the output fully low(it's getting low till 1.5V rather…
Part Number: SN74LVC1G07-Q1 Hi
Does the SN74LVC1G07QDCKRQ1 have safety documents?
I would like to know the FIT rate and the Failure Mode Distribution.
Thanks!
Chris
Part Number: SN74LVC1G07 Hi Team,
1. Could please explain what is Vload? How it becomes 2*VCC?
2. In our design we are using VCC as 5V. Since RL is 500ohm. Will it work if we give 10K pull up in the input?
Vinput = 5x(500/1500) = 1.6V <3.5V
Part Number: SN74LVC1G07-Q1 Hi TI Team,
We have found that the buffer is misbehaving in one of our boards. The output is 0-1V low-high, and the input is 0-5V. In this particular buffer even when the input is not given there is a voltage similar to output…