Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74AUP1G17 , SN74LVC1G17 , LM321LV Hi Sir,
I need a buffer/ driver to control my RF device but it need the isolation spec. at 2.4GHz~7.2GHz.
The input is CMOS/3.3V.
The drive capacity need 1.5mA…
Part Number: SN74LVC1G125 Hello, I have downloaded the model from the TI product page, and import it in OrCAD (import/PSpice/.cir, then open the .olb through the library). The simulation doesn't complete and indicates the error "Values must be monotonic…
Part Number: SN74LVC1G125 Hello,
Please verify the difference representation of DPW 5 from datasheet and package information
DPW 5 Package Information on datasheet, see pages of 19-25, DPW has 3D generated package and mechanical drawing.
https://www…
Part Number: SN74LVC1G125 Hi,
I would like to check with you is there any pull low inside the OE pin of SN74LVC1G125?
If customer leave OE pin floating, could it work normally?
Part Number: SN74LVC1G125
Hello,
SiliconExpert Technologies has been contracted by our customer to work with their suppliers to collect component information. We would appreciate your support to provide us with the required information indicated below…
Part Number: SN74LVC1G125-Q1 Hello Ti engineers,
there is a SN74LVC1G125-Q1 in our design,the OE is tie to GND ,and A is from outside device (SPI_MISO) , and Y connect to MCU ,we found that when A is tristate,Y is low,but MCU cannot control the AURIX_SPI3_MISO_3V3…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74AUC1G125
Hi, Support Team
We would like use SN74LVC1G125 support 125MHz at 2.5Vcc is workable?
if any, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: SN74LVC1G125 Hello,
I am looking for quality or reliability information of a part (CLVC1G125QDBVRQ1) that we are looking to be a drop-in replacement for the 1P1G126QDBVRQ1 tri-state buffer in the SOT-23 package. I originally submitted a quality…