Part Number: SN74LVC1G14 I am using this inverter (PN: SN74LVC1G14YZVR) in a design and I would like to simulate it in TINA. The only simulation models available from TI on the landing page for this component is an IBIS model, an HSPICE model and a behavioral…
Part Number: SN74LVC1G14 Temperature dependence of threshold voltages of SN74LVC1G14DB I measured with VCC = 3V @ 0°C @ 70°C Positive Threshold Voltage 1.681V 1.675V Negative Threshold Voltage 0.9V 0.938V Hysteresis Voltage 0.…
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74LVC2G86 Hi Sir,
My customer is looking for a single-channel inverter device shown below the figure, may I know if SN74LVC1G14 can meet the freq at 60~128Hz?
Part Number: SN74LVC1G14 Hello,
While testing this component, we found a very strange issue. The input is 0V constant (pulled-down to GND by a 100k resistor), but it takes the output around 700ms to go HIGH after the supply is connected. In the following…
Part Number: SN74LVC1G14 I downloaded the SGS report from TI's official website, as shown in the following figure. However, there are hidden parts in the file. Is there a public version available?
Part Number: SN74LVC1G14 Hi,
C an you justify the PDN for the part SN74LVC1G14DBV. In your website the series is active whereas we have the PDN and according to it the part is in EOL stage.
Herewith, attaching the PDN.
Regards,
Harshita
ThermFisher Sci…