Part Number: SN74LVC1G14 I am using 74LVC1G14SE-7 in my new design. Please provide the maximum and minimum of VIH and VIL for 74LVC1G14SE-7 as this is not specified in datasheet.
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74LVC1G17 , Hi,
if you look in the datasheets there is the Buffer https://www.ti.com/lit/ds/symlink/sn74lvc1g17.pdf on page 15 with the DPW / X2SON package at max. Op Temp with +125 °C.
And…
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74AHC1G14 , SN74AUP1G14 I use the device to shape a slowly changing signal in order to be able to process the signal with normal logic. During tests I came across a strange behaviour of the device…
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74HCS14 Page 4 of the data sheet says that the absolute maximum input voltage range is -0.5 to +6.5 volts. Note 2 says that the negative rating may be exceeded if the maximum input current rating…
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: LMV761 Hi all
My customer needs to implement a 3.7kHz (+/-300Hz) square wave oscillator to drive a buzzer and they are looking at the SN74LVC1G14.
Please refer to their schematic below.
Any other…
Part Number: SN74LVC1G14 My customer question below, I'd appreciate your advice.
currently I’m looking for some Logic IC’s. I want to establish a stable basis for our new device, which should be available for the next 10-20yrs.
Therefor…
Part Number: SN74LVC1G14-EP Hi there, what is the commercial equivalent for SN74LVC1G14MDBVREP?
I noted a "M" in the -EP part number...does that mean anything?
I believe the identical electrical match should be the following. Please confirm…
Part Number: SN74LVC1G14-Q1 Hi I'm doing an FMEA on my design and I have used a 74LVC1G14-Q100 Schmitt trigger inverter. ( single gate on a chip) I need to know what the MTBF figure is for this chip
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: SN74LVC1G17 , Kindly provide the output resistance graph wrt to output source and sink current for SN74LVC1G14 and SN74LVC1G17
Part Number: SN74LVC1G14 Other Parts Discussed in Thread: TLV3701 Customer would like to use the device SN74LVC1G14 to invert to a negative voltage between 0V and N3V. Input voltage with a mosfet of 0V-P3V3, invert to a negative voltage between 0V and N3V…