Part Number: SN74LVC1G34 Team,
Do we have the package outline (dimension information) of SN74LVC1G34DCKR? Customer is looking for such info, but looks like we only have info about some other packages only in the datasheet. Thanks.
As far as I know, a single manufacturing site does not change its lead frame. But it is possible to get devices from multiple manufacturing sites, even on the same reel.
Part Number: SN74LVC1G34 Hi, We are planning to use SN74LVC1G34 (Single 1.65-V to 5.5-V buffer) in our design.
We are using the IC in such a place where it will be working in down voltage translation.
Please find the working condition mentioned below, …
Part Number: SN74LVC1G34 Other Parts Discussed in Thread: TMUX1208 , Dear Team,
I am using SN74LVC1G34 to enable and disable TMUX1208. The control signal to SN74LVC1G34 will be coming from Arduino Nano.
Below is my circuit . May I know is it fine or not.…
Part Number: SN74LVC1G34 Other Parts Discussed in Thread: SN74LV1T125 , SN74AHC1G125 Hi there,
I would like to use the SN74LVC1G34 between 2 devices which communicate via UART (3.3V).
The devices will be separated by a long cable of 5 - 10 m and the max…
Part Number: SN74LVC1G34 Hi Team,
My customer wants to know block diagram of SN74LVC1G34. The block diagram is not obtained in our datasheet. Can you share the block diagram with my customer? Thanks a lot!
BR
Gust
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74LVC1G34 , SN74LV1T125 Hello,
I am currently using the SN74LV1T34 (DCK package) to shift a 3.3V PWM signal of a few MHz to a 4.096 level signal. This is then just low pass filter averaged and…
Part Number: SN74LVC1G34 Other Parts Discussed in Thread: SN74LVC125A , Hi Sir,
As the title, our customer is seeking for the redriver or buffer solution which can increase the driving capability for the long trace around 10000 mils.
Please help to recommend…
Part Number: SN74LVC1G34 Hi TI team,
Is there any characteristics for the source and sink current with respect to VCC.
If not available, could you please share the source and sink current ratings at VCC = 4.9V and 5.1V.
Thank you in advance.