Part Number: SN74LVC1G66 Hi,
Do you have the Pspice or TINA TI Model for the device SN74LVC1G66? My customers would like to do the simulation with the model. There are only Hspice model online, what are the differences, can it also be used with Pspice…
Part Number: SN74LVC1G66-Q1 Other Parts Discussed in Thread: TS5A3166-Q1 Hi there,
I'm planning to use the component as a reset switch for an integrator stage opamp.
The max voltage on the integrator capacitor is 3.3V, C=20n, and the reset integrator…
Part Number: SN74LVC1G66-Q1 Hi Expert,
May I know if there is any data for the leakage current of SN74LVC1G66QDCKRQ1 in high humidity environment?
Is there any humidity test performed and can you share the test report?
Thanks!
Ethan Wen
Part Number: SN74LVC1G66 Other Parts Discussed in Thread: TS5A3167
Hi team,
Customer ask if SN74LVC1G66 can support power down protection which means that there is no problem even if the voltage hots the terminal when the power is off.
Best regards,…
Part Number: SN74LVC1G66 Other Parts Discussed in Thread: SN74AUC1G126 , SN74LVC1G126 Hi Sir,
Our customer encountered the problem that the used SN74LVC1G66 on SPI CLK switch, but they meet the CLK will getting distortion.
Could you please help to check…