Part Number: SN74LVC2G00 Hi there Datasheet, page 3 are the pin configurations. For YZP package (DSBGA) the pins are named as 1, 2, 3, .....
Page 17: footprint pins are defined with A1, B1, ..... .
What is the correct pin naming for SN74LVC2G00YZPR?
…
Part Number: SN74LVC2G00 Hello guys,
One of my customers is considering using SN74LVC2G00 for their next products.
At this moment, they have the following question about this device datasheet. Could you please give me your reply?
Q1. On page 8 of SN74LVC2G00…
Part Number: SN74LVC2G00 Hi Team,
I am working on a prototype as the following pciture, but not sure if Nand gate output pin has the capacity to control optocoupler vol617a, or I need to add a MOSFET to drive the optocoupler, can someone help advice, thanks…
Part Number: SN74LVC2G00 Hello team, can you help with the below. Thank you!
In table 7.5
1) In the SN74LVC2G00 data sheet there is an Ic and delta Icc. What is deltaICC? Should it get added to the Icc value to compute total power dissipation?
2) Are…
Part Number: SN74LVC2G00 Hi team,
My customer is using the SN74LVC2G00 now and find the negative overshoot (-0.9v) is over the device spec -0.5V, But the time is very short(80us). We want to check whether it has risks here? Thanks.
There are current-sense amplifiers with a (latching) alert output like the INA381 or INA300. But you probably do not need their differential inputs, and their minimum amplification might be too high.
Alternatively, build a set/reset latch from two NAND…
Part Number: SN74LVC2G00 Other Parts Discussed in Thread: TINA-TI , , SN74LVC2G02 Tool/software: TINA-TI or Spice Models Hi,
I'm looking for Spice model of SN74LVC2G00 and SN74LVC2G02.
Thanks,
Vinayak
I think the easiest way to build this would be to simply combine the comparator with an actual set/reset latch, i.e., CD4043B or CD4044B, or made from two NAND or NOR gates (SN74LVC2G00/SN74LVC2G02).
NAND: SN74LVC2G00 AND: SN74AHC08 (The AHC propagation delay at 3.3 V is marginal. If this is important, use 2× SN74LVC2G08.)
This logic function (AND with one inverted input) could be implemented with just the SN74LVC1G97, but would require four…