Part Number: SN74LVC2G07-EP We are using your SN74LVC2G07MDCKTEP part in some boards we are doing thermal analysis on and need additional information that is not in the datasheet. The datasheet lists thermal impedance as 259°C/W but it doesn't say where…
Part Number: SN74LVC2G07 Hi,
For the part SN74LVC2G07DCKT, I am looking for the output capacitance.
The datasheet provides the Ci which is 3.5pF.
But it doesn't provide the output pin + driver capacitance when a steady 3.3V is driven out.
Is it a…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: TXU0102 , SN74LVC2G34 Hi Team,
can the SN74LVC2G07DRY be used to buffer two clock lines that are 5 V level and to convert them to 3.3 V as well?
What is the skew between the two devices? E.g., if one…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74LVC1G07-Q1 Hello,
Could you confirm if the component SN74LVC2G07DBVR is an automotive part (AECQ) or not please?
Best regards
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74LVC2G32 , SN74LVC2G125 , SN74LVC1G97 Hi,
Customers need Dual Buffer with Open-Drain outputs, such as SN74LVC2G07, but with enable function. I only found Dual buffer (3-state output) with enable…
Part Number: SN74LVC2G07 Hi experts,
My customer is using SN74LVC2G07 to generate two 1.8V clock signals from a 3.3V clock signal (from DSP). The simplified schematic is shown below:
Phenomenon: The output high-level voltage is measured as around 1.2V;…
Part Number: SN74LVC2G07 Other Parts Discussed in Thread: SN74AUP2G125 , SN74LVC2G125 , SN74AUC2G125 Hi,
We are using the ADC which supports 3 wire SPI communication and we are using SPI level shifter which will convert the 4 wire SPI communication from…
Part Number: SN74LVC2G07 Hi Team,
Kindly need your help to check what is the different for below 2 body marking? I can only find "CV" in the DS. Kindly advise what does the body marking on the part represents? How to read the body marking? Thank…
Part Number: SN74LVC2G07 Hi,
I'm working on a complex system with long trace length (>60inches) on Jtag signals, so I would like to add a buffer on it.
Wondering knows which parameter of the buffer(maybe SN74LVC2G07 or GTL2014? ) will be the key factor…