Part Number: SN74LVC2G53 Hi team, regards to sn74lvc2g53, I have 2 questions coming from my customer.
1.What the purpose is for the COM pin?
2.If not using the COM pin, how to deal with it, floating, pull high or pull low?
Part Number: SN74LVC2G53 Hello expert,
Could we have the comparison table between SN74LVC2G53DCUR and NLAS1053USG? Also pin 3 has difference between ours and on-semi's. Could we have a co-layout recommendation? Or we can just leave pin 3 open? Thanks a…
Part Number: SN74LVC2G53 Other Parts Discussed in Thread: TS5A3154 Hi Team,
What is the difference between SN74LVC2G53DCUR and TS5A3154DCUR?
They look like P2P solution and I only see the bandwidth is differential, SN74LVC2G53 is 300MHz and TS5A3154 is 100MHz…
Part Number: SN74LVC2G53 Hi Team,
My customer would like to use PWM signal(about 100kHz) on SN74LVC2G53. For the frequency response of SN74LVC2G53 , does it mean SN74LVC2G53 can support frequency up to MHz according to VCC?
Best regards,
Hardy
Part Number: SN74LVC2G53 Team,
Do we have other Logic option that would be dropped-in replacement for the below? The idea is to use newer TI families that could be slightly cheaper.
SN74AHC1G04DBVR SN74LVC2G53DCTR
Thanks in advance,
A.
Part Number: SN74LVC2G53 Other Parts Discussed in Thread: SN74LVC1G98
Hello
I'm using a MUX to implement a certain digital logic which has states A, B, and C. The truth table is as follows:
Inh: enable disable MUX
A: Switch
Com: in my case, input…
Part Number: SN74LVC2G53 Other Parts Discussed in Thread: SN74LVC1G04 Hi E2E,
Could you kindly provide the theta JC of SN74LVC2G53?
BTW, Could you kindly provide TJMAX of SN74LVC1G04?
Thanks!
Other Parts Discussed in Thread: SN74LVC2G53 Hello TI,
According to the 'Features' summary on page 1 of sces324n, the SN74LVC2G53 supports the Ioff feature, but Ioff is not mentioned under 'Electrical Characteristics' on page 4. What is the max…
Other Parts Discussed in Thread: SN74LVC2G53 as pspice model is not available for SN74LVC2G53. i want to use it in my circuit. Biasing the IC under 5V vcc and Gnd. sensor is attached to the COM pin of demux and Y1 , Y2 are connected to different ADC. IH…