Part Number: SN74LVC3G07-Q1 Hello,
I am referring to the functional safety information document provided for the part number "SN74LVC3G07QDCURQ1" for internal analysis. It looks like the addition of the Failure mode distribution is not making 100%. Maybe…
Part Number: SN74LVC3G07-Q1 Dear TI Experts,
in a cost sensitive product there is a 3V3 sensor providing digital signal for a 5V uC , I would like to translate voltage levels with an open drain buffer SN74LVC3G07-Q1:
To calculate the Rp value I would…
Part Number: SN74LVC3G07-Q1 Hello, I accidentally used a downloaded footprint which resulted in the Input and Output for SN74LVC3G07-Q1 to be flipped. I am hoping that someone can please help me find a similar package offering that has the input and output…
Part Number: SN74LVC3G07-Q1 Other Parts Discussed in Thread: SN74LVC2G17-Q1 , SN74LV125A-Q1 , SN74LVC3G07 , SN74LVC3G34 Hello,
Will the output of this device be 0V when the Vcc is 0V while the input is set to 3.3V?
I saw that the device's input is rated for…
Hi Delaney,
The SN74LV1T08 is the only option we currently have available for a single supply up-translating AND gate.
If open-drain is an option, then a pair of open-drain buffers can be used as an AND gate (directly connect the two outputs together…
Part Number: SN74LVC1G07-Q1 Other Parts Discussed in Thread: SN74LVC3G07-Q1 , SN74AVCH8T245 , SN74AVC8T245 Hi experts,
We have a customer that is looking for 10-15mA source/sink at 1.8V. I see lots of buffers that support the 1.8V level but the max current…
Part Number: SN74LVC07A-Q1 Other Parts Discussed in Thread: SN74LVC3G07-Q1 Hello all,
I would like to know the high-level input voltage of this device when the supply voltage is 5V. Why I would like to know is to use this device as a voltage translator…
Part Number: SN7407 Other Parts Discussed in Thread: SN7417 , , SN74LVC2G17-Q1 , SN74LVC1G07-Q1 , SN74LVC1G17-Q1 , SN74LVC3G07-Q1 , SN74LVC07A-Q1 Is there an identical part to the SN7407 and SN7417 that are AEC-Q100 Qualified? If not what are the closest alternatives…