Part Number: SN74LVC3G17 Hi, I would like to check if the following information is available for SN74LVC3G17DCUR ( https://www.ti.com/lit/gpn/SN74LVC3G17 ):
Junction-to-Board (Theta_JB) thermal resistance:
Junction-to-Case Bottom (Theta_JC, Bottom) thermal…
Part Number: SN74LVC3G17 HI
The physical marking of this product is not consistent with the sample in our warehouse, and the verification specification is also inconsistent. Please confirm whether the marking of the following materials is correct and…
Part Number: DRV5013 Other Parts Discussed in Thread: SN74LVC3G17
Hi,
Q1. I would like advice on what to look out for when connecting DRV5013 to SN74LVC3G17. We need you to check the external components. <Conditions> ■ Operating temperature: 5~80°…
Part Number: SN74LVC3G17 Other Parts Discussed in Thread: SN74LVC1G17 Hi Team,
This inquiry is related to the other E2E thread below.
e2e.ti.com/.../10-mhz-ttl-transmitter-and-receiver-ic
According to our customer,
If I was going to use the 74LVC3G17 for…
Part Number: SN74LVC3G17 Hi Team,
We are using the SN74LVC3G17DCUR Buffer part in our schematics. I had attached the schematic Image below, Kindly review the schematics and share your valuable feedback with us.
Thanks and Regards
- Teja
1. Yes.
2. Two filters would combine to reduce the maximum frequency.
Please note that traces and cables have a capacitance of very roughly 1 pF/cm, so 2 m will result in about 200 pF, so you can reduce or omit the discrete capacitor, and have a smaller…
Part Number: SN74LVC3G17 Dear Team,
Can you please advise what is the Vt+ for 5V ?
On our datasheet table 6.2 we define the Vt+ for 4.5V to be 2.19Min and for 5.5V to be 2.65V
Would it be correct to make a linear extrapolation and assume that at 5V we…
Part Number: SN74LVC3G17 Hello expert, I'd like to get about Reflow, flow, had soldering requirement for SN74LVC3G17DCUR. For reflow requirement, I found following documents as general TI's recommended reflow requirement. https://www.tij.co.jp/jp…
Part Number: SN74LVC3G17 Hi, customer had a question on the datasheet for SN74LVC3G17DCURG4 and have a question about switching characteristics in section 6.6. What is the differences between the two rows? Both test conditions refer to Figure 3. Should…
Part Number: SN74LVC3G17
I tried to simulate schmitt trigger using Ltspice and the given photo is the output with the circuit. The output does-not align with the values given in the data sheet. May i know on what changes to make to get output as per…