Part Number: SN74LVC3G34
Hi team,
Could you check the marking for SN74LVC3G34DCUR? The customer found two different types marking. One is only one line another is two lines.
The datasheet listed below, what does it mean?
(34, C34J, C34Q ,C34R)
(CR, CZ…
Part Number: SN74LVC3G34 Hi team, Kindly assist us with below mentioned query.. 1] For part series SN74LVC3G34DCTR under the thermal data only thermal resistance of junction-ambient is present . we need the value of thermal resistance of junction-case and…
Part Number: SN74LVC3G34 Hi team,
Could you please kindly help check the time delay for different channels?
We can only find tpd on the DS.
Thanks,
Brian
Part Number: SN74LVC3G34 Hi Team,
I am using SN74LVC3G34DCUR in my design. I would like to get the schematics design reviewed by experts. Attached the schematics review. SN74LVC3G34DCUR.pdf
Part Number: SN74LVC3G34 Other Parts Discussed in Thread: SN74LVC07A , SN74LVC32A , SN74AHC126 , SN74ALVC126 Hi team.
My customer want to find a buffer to boost SGPIO signal.
The picture above is the standard SGPIO signal. My customer uses it for communication…
Hello,
In addition to the recommendation above, there is a newly released device that is optimized for SPI buffering or level shifting:
https://www.ti.com/product/TXU0304
https://www.ti.com/product/TXU0304-Q1
It can support 1.1 to 5.5V supply configurations…
Part Number: SN74LVC3G34 Other Parts Discussed in Thread: SN74LVC2G17 , UCC27517 , SN55451B , SN75451B , UCC27517A-Q1
Hello,
I am using the buffer to drive optical transmitter which can require a current upto 96mA in worst case. As per the datasheet the current…
Part Number: SN74LVC3G34 Hello,
I am using the SN74LVC3G34 buffer to connect an SPI bus to a RAM.
What I am observing is that the buffer output signals decrease over time, which causes the RAM to fail when processing the data. I have tried different SPI…
Part Number: SN74LVC3G34 Other Parts Discussed in Thread: SN74LVC3G17 Hi Sir,
Do we have schmitt trigger which is pin to pin compatible with SN74LVC3G34DCTR?
And the schmitt trigger can support SPI interface.
Thank you.