Part Number: SN74LVC573A Hello Team,
Currently my customer has some design guide and SN74LVC573A working mechanism questions, could you please help with it? Thanks!
Q1: What's the recommended connection of the signal pins, floating, pull up or pull down…
Part Number: SN74LVC573A Other Parts Discussed in Thread: SN74AHC573 , SN74AC573 , SN74LV573A , SN74HC573 Hi Experts,
The part SN74HC573NSR is obsoleted. So we have to find a p2p replacement.
I noted the only p2p and package compatible device is SN74LVC573ANSR…
Part Number: SN74LVC573A Hi,
We are using SN74LVC573ARGYR in various designs. We found a phenomena and we intend to check if issue is being familiar with such a scenario by TI / or cy customers.
In a specific design, one of the inputs (D6) is connected…
Part Number: SN74LVC573A-Q1 Dear team,
We are using this part ( SN74LVC573AQ1 ) in one of our projects,
1. We want to know if the latch output enable pins are left open and Latch enable is low, what will be the output state of the Latch - upon Power State…
Part Number: SN74LVC573A-Q1 Do you have an IBIS or Spice model for SN74LVC573AQPWRQ1? I would like to simulate cross-talk and signal quality of my PCB while using this component.
Part Number: SN74LVC573A Hi Team,
According to SN74LVC573APW datasheet, my customer has a concern about the temperature.
Operating free-air temperature: –40 to 85 °C
Op Temp: -40 to 125 °C
Is it a missing or Operating free-air temperature different…
Part Number: SN74LVC573A Hello,
is the SN74LVC574ARGYR qualified for Ta -40°C to 125°C ?
On page 2 in the datasheet -40°C ..85°C is specified for VQFN20 package (this is the RGY type)
On abbendum page 2 the datasheet specifies -40°C…
Part Number: SN74LVC573A Other Parts Discussed in Thread: SN74LVC574A Hi, Team,
My customer find there is some output issue for the SN74LVC573A. Could you help check it?
Issue: When output a low level voltage for the SN74LVC573A, there is some oscillation…
Part Number: SN74LVC573A hi dear supporting team,
what's the max junction temp of SN74LVC573APWR? there is no information in d/s. and from calculation, the max power consumption at 3.6V is only 0.036mW, is this correct? tks!