Part Number: SN74LVT245B Dear Team,
Could please share the below information?
1. Shock and Vibration test data
2. Life cycle survey
Supplier
Supplier Part Number
Component lead time
Supplier Est for Part Life Cycle Phase
( Introduction/Growth…
Part Number: SN74LVT245B
Hi,
That datasheet says the following:
"To ensure the high-impedance state during power up or power down, OE should be tied to VCC through a pullup resistor; the minimum value of the resistor is determined by the current…
Part Number: SN74LVT245B
We have been using the SN74LVT245BPW to transmit switching signals ranging from 200kHz to 35MHz. The input is driven directly by a Cyclone V FPGA at 3.3V and the output drives the input of an isolator IC with 125Ω thevenin resistor…
Part Number: SN74LVT245B Is there a clamp diode on the 245 pin? BB0~BB7 of A1~A8 are key signals, and FPGA_BB0~FPGA_BB7 of B1~B8 are FPGA input signals. 245 will be damaged when the button is pressed live. In series with a 100Ω resistor between BB0~BB7…
Part Number: SN74LVT245B Hi,
I want to add pull up resistor in the input side for 5volt.
Can you please help me to select a pull up resistor value limit?
Thank you in advance.
Part Number: SN74LVT245B Other Parts Discussed in Thread: SN74LVC245A Hi,
Now I'm studying how to calculate power consumption of logic devices. I checked FAQ in logic forum and checked app note SCAA035B. Then I studied that Dynamic power-dissipation…
Part Number: SN74LVT245B We are using the Component (Part No.:SN74LVT245B), it is working working fine. But, the requirement is as attached. Please mention any Bus transceiver for the following specifications as attached.
Best Regards,
Chaithra
Part Number: SN74LVT245B Other Parts Discussed in Thread: SN74LVC245A , SN74LVCR2245A Dear Sirs,
I want to use the SN74LVT245B level shifter in order to protect my processor from backpowering on a RGMII interface. The processor, which has its own power…
Part Number: SN74LVT245B Other Parts Discussed in Thread: SN74LVTH16374 Hi team,
My customer plan to use our SN74LVT245, they want to know the maximum data rate that SN74LVT245 can support, can you help check this? Thanks a lot!
BTW, would you pls let…
Part Number: SN74LVT245B Other Parts Discussed in Thread: TXS0108E , TXS0101 , TXS0104E Hi,
I have designed the circuit using the IC 74LVT245 to convert 5V to 3.3V. The output of hall sensor is open collector, that is connected to the input side of the 74LVT245…