Part Number: SN75C1167 Dear Specialists,
My customer is considering SN75C1167and has a question.
I would be grateful if you could advise.
---
In the electrical characteristics ICC item, when VI = 2.4 or 0.5 V, the TYP value is 5mA and the MAX value is…
Part Number: SN75C1167
Hi,
On my customer's board, when VDD=0V on SN75C1167, it is possible to supply some voltage on 2D pin, DE pin and 1D pin. What issues does they have? Is any damage occurred? Please let us know your comments.
Thanks and best…
Part Number: SN75C1167 Hi team,
I think the drive current will flow 50mA when the power supply is 5V and the termination resistor is 100Ω connected. But is it limited to 20mA by the clamp current (Iok)? If the instantaneous drive current exceeds 150mA…
Part Number: SN75C1167 Hi Sir,
Customer used the SN75C1167 for the UART signal design, now they have made a testing method but they encountered a behavior but not sure it is abnormal or not.
They simple test the chip only, without any pcb and not connect…
Part Number: SN75C1167 Hi,
May I ask if we are able to improve the slew rate of transceiver?
Please refer to the capture below, the transceiver output is at CH3
Please let us know if further information needed.
Thanks for your help.
Part Number: SN75C1167 Hi Team, Recommended operating condition of driver output current shows the following. question1) Is ±20mA defined as per single driver? I believe it but would like to confirm just in case. question2) What is concern if output…
Other Parts Discussed in Thread: SN75C1167 Hello,
I was wondering is there a reason to connect the differential receiver inputs on SN75C1167 (1A and 1B for example) via a small resistance (~100)? If so can you explain why. If not, then please verify that…
Part Number: SN65C1167 Other Parts Discussed in Thread: SN75C1167 , SN7534050 JEDEC document JEP155 states that 500-V HBM allows safe manufacturing with a standard ESD control process. Most parts mention HBM / CDM immunity in some way or another.
But the…
Hi Team,
Could you please tell us what to do with the unused Driver/Reciver pins ?
Driver : 2D, 2Y, 2Z Receiver : 2R, 2A, 2B
The answer for receiver was in the following URL. http://e2e.ti.com/support/interface/industrial_interface/f/142/p/102795/361353…