Part Number: SN75DP149 Hi TI Teams,
One of our customer reported that the monitor connected to the HDMI output port of DP149 has not display during the aging test, and the display can only be restored if the uplink port is re-plugged. The aging time is…
Part Number: SN75DP149 1. If the product works with the NVDIA GeForce RTX4000 graphics card and some monitors are connected, the screen may be splintered after hot swap.
2.The product display doesn't wake up the image automatically with matching signal…
Part Number: SN75DP149 Hi TI Teams,
We encounter abnormal temperature rise problem when using SN75DP149, the temperature can reached up to 100℃ when it working, which will lead to some abnormal display problems under specific conditions. Can u help to…
Part Number: SN75DP149 Hi,
in an existing design I need to replace a SN75DP139RGZ with and SN75DP149RSB. Space-wise this is not an issue, also the answer given here
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/635028/sn75dp149…
Part Number: SN75DP149 Hi,
We are looking for the eDP/DP to HDMI conversion solution, we found that SN75DP149 can change the DP++ to HDMI. But i am not sure about DP. Can you help me to find one solution for this? Video=FHD capable
Thanks and Regards…
Hi,
1. There are lane0/1/2 on EyeScan settings of EyeScan tool. I think that lane0/1/2 are matched with IN_D0/D1/D2(Pin7 to Pin1) of SN75DP149. Is it correct?
This is correct
Thanks
David
Part Number: SN75DP149 Other Parts Discussed in Thread: TDP158 Hi Sir,
As the topic, our customer would like to co-lay with SN75DP149 & TDP158...looks the package size and pinout be same, just need your support to re-confirm it workable? And any suggestion…
Part Number: SN75DP149 Hi, Sir,
Core chip is VMM3332,
1. from VM3332 signal output, HDMI 4K30Hz is OK.
2. from VM3332 signal output DP++, transfer by SN75DP149, 1080P60Hz is ok, but 4K30Hz will blinking in most PC.
Are there any suggestions to support…
Part Number: SN75DP149 The VIDEO output from DP to HDMI is normal. The PC side can recognize the TV'S EDID normally, but there is no audio output.There is only one audio output option on PC, so the audio output option of TV cannot be found. HU-1PS…
Part Number: SN75DP149 Hi,
Just doing some test layout work to check the pinout. I notice that the 75DP149 outputs are backwards with reference to the DVI connector. I am using this connector as I need to analog outputs as well.
Q1) The swap function…