Hi!
I might be missing something, but whenever I search for the TMS320C64x Image Library, I end up at this site, where I supposed to find a download link:
http://www.ti.com/tool/sprc094
Matter if fact is, that there are only 2 pdf files to download, but…
Hi,
This C64xIMGLIB library can be build with C6000 code generation tools and not with ARM toolchain like using Linux Makefile etc.,
http://www.ti.com/tool/sprc094
If you are using ARM+DSP processor like OMAPL13x then you can use SYSLINK or DSPLINK for…
As i am not familiar with c64x+ core which you say is the next higher revision chip of c64x core.
Could you introduce for me ,
I know dm642 belongs to c64x core,
which chip belongs c64x+ core, 6467 or something link that?
And what C674x belongs to
currently…
Walter,
Although it takes 16-bit parameters, the DSP_dotprod() function in C64x+ DSPLIB is a good start:
http://focus.ti.com/docs/toolsw/folders/print/sprc265.html
To further explore the capabilities of parallel multiplication in C64x+/C674x architecture…
Hi, Can anyone help me to use the dilation & erosion function in the c6400 IMGLIB? I'm using v1.04b as can be found on the TI website (SPRC094). For example, I have:
image_thr(pingPongBufferA, pingPongBufferB, capture_imageCols, capture_imageRows…