Hi Dean,
Under the SPRC133, there are two packages:
1. C55XCSL-SPRC133 — Download TMS320C5500 Chip Support Library (for C5501, C5502, C5509, C5509A, and C5510, C5510A) : C55XCSL-SPRC133 Driver or library | TI.com
2. C55XCSL-LOWPOWER — TMS320C55x…
Hi Guntupalli,
You will need to download the SPRC133,
C55XCSL-LOWPOWER — TMS320C55x Chip Support Library for C5504/05, C5514/15/17 and C5535/45 devices from
SPRC133 Driver or library | TI.com
and the dependencies:
Release 3.08.01 Dependencies
===…
Hi Dean,
I do not know the dependency for the C55XCSL-SPRC133 i.e. the DSP/BIOS version and CGT tool version etc. I will forward this thread to SDTO team for further help!
Best regareds,
Ming
Hi There,
There is a TI design for this application: http://www.ti.com/tool/TIDEP-0077 . Here is the design guide ( TIDUCY1C.PDF ).The source code for the audio-preprocessing is in the C55xx CSL Low Power 03.08.00. You can download it from: SPRC133 Driver…
Hi Guido,
All the EMIF examples are at c55_csl_3.08.01\ccs_v6.x_examples\emif. You can find the C55x Low Power CSL at SPRC133 Driver or library | TI.com .
The documentation about the C5517 EMIF is in chapter 4 of C5517 TRM: TMS320C5517 Digital Signal Processor…
Hi Jim,
The other differences are that I was using the following:
C55x CSL 03.08.01.00: SPRC133 Driver or library | TI.com
CCS 10.40
DSP/BIOS 5.42.00.07 and DSP/BIOS 5.42.02.10
CGT for C5500 4.4.1 Best regards, Ming
Hello Pedro,
You should review the Secure Digital Input Output (SDIO) Specification V2.0 which is one of the industry standards followed by the MMC/SD card controller.
Details for speeds and memory sizes should be included in those industry standards. …
Hi Katherine,
Support for C5000 is limited, please see: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/818771/faq-support-guidance-for-c5000-digital-signal-processors
I suggest you check the CSL for McBSP example code: https…
Gibbs,
I misunderstood your requirement concerning Linux. I thought you needed Linux on the device. I understand now you need the USB audio class device to communicate with a Linux host.
The C5535 DSP might meet your needs.
The C5000 Connected Audio Framework…
Hi Yoshiyuki,
yoshiyuki sekine said: The structure is "PLL_Config". I find a define of the structure "PLL_Config" in "csl_pllB.h". But, there in no member named "clkmd0".
This means your application has a dependency…